STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HardFault during HAL_SPI_Receive_DMA()

Posted on November 29, 2015 at 14:15 Hi, just a quick note: HAL library: F2 v1.1.0 (09/Oct/2015) I was trying to use this function and have encountered hardfault when the size is >1. I did not look deep into the problem, but the cause...

the by Associate
  • 950 Views
  • 0 replies
  • 0 kudos

Is there a simple sample code for USB

Posted on November 27, 2015 at 09:34Hi, I got the Cube firmware from ST, and I cannot found the USB sample code for test purpose. The current demo codes are complicated, I have to put App, middleware and driver to make the USB work, and it is not go...

jeff23 by Associate II
  • 1850 Views
  • 3 replies
  • 0 kudos

STM32F429 USB Host

Posted on November 01, 2015 at 19:28 Hey guys, I've been trying to create USB FS host drivers for a vendor-specific device on the STM32F429 Discovery board. So far I've not had any luck getting ANY device (be it from the MSC, HID or Vendo...

STM32f401 Discovery I2C + External Interrupt

Posted on November 24, 2015 at 17:24Hi, I am working on a project where I am communicating with a capacitive touch sensor via I2C.  I have successfully achieved read/write over I2C , and now I would like to use the external device's interrupt line t...

Bootloader PC s/w for USART STM32F3

Posted on November 24, 2015 at 14:24Is there any off the shelf PC bootloader s/w that can take the output from IAR EWARM and load it via a USART on an STM32F303?  #stm32 #uart #bootloader

gbigden by Associate III
  • 1099 Views
  • 2 replies
  • 0 kudos

USB connection ends with TXERR

Posted on September 23, 2015 at 21:04Hi there forum,I would like to connect a USB pen to my STM32F4-Discovery kit.I am using libraries from stsw-stm32068.zip, and the GPIO, USB initialization code and the usb_conf.h and usbh_conf.h files are from Au...

Emmil by Associate II
  • 1617 Views
  • 2 replies
  • 0 kudos

BUG in STM32L4 Hal lib (v1.1) hal_sd.c

Posted on November 21, 2015 at 16:01Hello everybodyI have found a BUG in STM32L4 hal lib (v1.1)I don't know if it is present in other STM32 family hal library.in stm32l4xx_hal_sd.c file at 1657 linepCardInfo->CardCapacity  = ((pCardInfo->SD_csd.Devi...

fra by Associate II
  • 1584 Views
  • 3 replies
  • 0 kudos