Skip to main content
the
Visitor II
November 29, 2015
Question

HardFault during HAL_SPI_Receive_DMA()

Posted on November 29, 2015 at 14:15

Hi, just a quick note:

HAL library: F2 v1.1.0 (09/Oct/2015) I was trying to use this function and have encountered hardfault when the size is >1. I did not look deep into the problem, but the cause seems to be on the line 16 (code below). Notice that the

HAL_SPI_TransmitReceive_DMA()

function is called using repeated ''pData''. Workaround is to use

HAL_SPI_TransmitReceive_DMA()

directly in application, using separate buffers. If anyone has some insight or explanation to this issue, please provide here. Thank you :)


HAL_StatusTypeDef HAL_SPI_Receive_DMA(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size)

{

......


/* Configure communication direction : 1Line */

if
(hspi->Init.Direction == SPI_DIRECTION_1LINE)

{

SPI_1LINE_RX(hspi);

}

else
if
((hspi->Init.Direction == SPI_DIRECTION_2LINES)&&(hspi->Init.Mode == SPI_MODE_MASTER))

{

/* Process Unlocked */

__HAL_UNLOCK(hspi);


/* Call transmit-receive function to send Dummy data on Tx line and generate clock on CLK line */

return
HAL_SPI_TransmitReceive_DMA(hspi, pData, pData, Size);

}


......

}

#hardfault #spi #dma #hal
This topic has been closed for replies.