STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 FatFs middleware problem with f_open();

Posted on December 24, 2015 at 02:34Would like to know if anyone comes across pointer crash when using f_open()?Background:Our project's configuration include FatFs and USB Host, and the LSE and HSE are 32.7KHz and 8MHz respectively. The media used ...

suilarso by Associate II
  • 3178 Views
  • 6 replies
  • 0 kudos

STM32 HID with HALL

Posted on December 27, 2015 at 21:37 Hello, i am creating car headunit from tablet, and USB OTG functionality allows to control tablet with STM I would like to get few commands, like SLEEP, WAKE, volume up/down, pause, play, next song, p...

STM32F072-Discovery Virtual Com Problem

Posted on December 25, 2015 at 19:48 Hi, I've been struggling to make a working program, that would allow my board to communicate with the computer. So far I reviewed a lot of examples but I still have problems to do so. I managed to connect the...

cravaour by Associate II
  • 1036 Views
  • 1 replies
  • 0 kudos

STM32F042 USB VCP not working

Posted on December 10, 2015 at 06:49I have generated code with STM32CubeMX which should enable VCP support for STM32F042, but USB still doesn't work. Until USB device is initialized in code, windows shows device as ''Unknown USB Device (Device Descr...

ajargans by Associate II
  • 4383 Views
  • 9 replies
  • 0 kudos

Dual CDC with STM32_USB-FS-Device_Lib_V4.0.0

Posted on December 24, 2015 at 08:25Hello,Is there anybody who have Dual CDC  keil project with usb library v4.0.0?I have dual cdc example v3.1.1 but it have a bug when send data  usart to usb.I tried to change v4.0.0 to dual myself by help of this ...

Bug in HAL_PCD_Init: Wrong HBSTLEN value

Posted on August 14, 2015 at 22:23I have been writing my own USB driver. While debugging an issue with the receive buffer/receive fifo I came across this issue.I am using an STM32F205VCT processor with an external HS Phy (USB3300). The function HAL_...

USB DFU Customised

Posted on August 30, 2012 at 01:00Hi, I would like to create a USB DFU device and host that can only talk to each other. What I want to do is to put a sort of flag such that my device will not be able to send its device descriptor to the host unles...

zoro7117 by Associate II
  • 3488 Views
  • 7 replies
  • 0 kudos