STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[HELP]STM32F4-DISCOVERY with MP3 Player

Posted on March 02, 2016 at 08:02Hei thereIs there any working mp3 player using this eval board ?Right now I try helix mp3 decoder but cannot compile using keil v4.There are some error on assembly.h i cannot understand.Please guide me thanks. #mp...

dree86 by Associate II
  • 7979 Views
  • 16 replies
  • 0 kudos

Run Nucleo only with power, no PC USB connection

Posted on September 01, 2016 at 18:33Hy, I start to work with the Nucleo Platform. I have several Nucleos and can program them with System Workbench for STM32, no problem. But when I connect the USB cable to either a USB power pack or a PC that has ...

harald by Associate III
  • 1737 Views
  • 2 replies
  • 0 kudos

Problem with ethernet

Posted on August 31, 2016 at 10:23Hi, I'm using STM32F746-DISCOVERY. I want to use ethernet, but I connect for a little time 3-4 seconds and the the connection dropped. When I try to connect again I cant. I saw the example of ST and there isn't any ...

STM32F1 USB interrupts, why LP and HP?

Posted on August 30, 2016 at 13:11Given that in some instances both interrupts can be active at the same time, what is the point or use in having two? Is there any reason why the vector table for both shouldn't point to the same interrupt routine su...

Mikexx by Associate II
  • 2540 Views
  • 1 replies
  • 1 kudos

USB Init fails on AHB Idle not set

Posted on August 29, 2016 at 19:43STM32F427.I cloned a cube project for a working application with Micrium os.  I want to run code without an OS.  As far as I can tell so far I am doing all the same initializations but the function USB_CoreReset fai...

USB FS Losing word in RxFIFO (STM42F40x)

Posted on March 03, 2012 at 06:09Hi All I thought that I had managed to tame the USB FS device, but I was wrong. There is one simple thing that is not working and it is so simple that it seems impossible to solve... I have a CDC class operating. Enu...

hpipon957 by Associate III
  • 4884 Views
  • 10 replies
  • 0 kudos