STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476G-EVAL Bootloader UART/CAN issues

Posted on July 22, 2016 at 12:07Hello together,I just want to find out how to use the basic bootloader operations on an STM32L476G-EVAL board. I read all the application notes (AN2606, AN3154, AN2557, AN3156) and the manuals for the board and the MC...

STM32 USB Full Speed Device Library

Posted on March 28, 2013 at 14:43It seems STM finally succeeded in their quest to make information about MCUs unsearchable. I can find a manuah for STM32 FS-Device development kit, but can anyone point me to the library itself (I need it with exampl...

eltar by Associate III
  • 6148 Views
  • 11 replies
  • 1 kudos

bug: STM32Cube, flash operation

Posted on October 10, 2016 at 16:05Dear all,using the flash and option byte functions from STM32CubeF4 (MCU: STM32F469) I am concerned about its implementation.Does anyone from ST may check the following code:1)stm32f4xx_hal_flash.c: line 592 - 598,...

STM32F7 Discovery - lwIP problem

Posted on October 11, 2016 at 15:19 I am using the STM32F7 discovery as a HTTP server with lwip and FreeRTOS. It is able to receive and respond to the HTTP requests without any issue until it attempts to respond to the 19th request where it take...

ADC with HAL, EOC flag never set

Posted on October 11, 2016 at 11:54Hello I am trying to use the ADC like this:ADC_ChannelConfTypeDef sConfig;  adc.Instance = ADC1;  adc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;  adc.Init.Resolution = ADC_RESOLUTION_12B;  adc.Init.ScanCon...

Send SERIAL_STATE with STM32CubeMX USB CDC driver

Posted on April 20, 2016 at 12:25Hello, In order to send SERIAL_STATE over USB IN interrupt endpoint I had to increase the CDC_CMD_PACKET_SIZE to 10 in usbd_cdc.h. Is there a way to do this in cubemx ? I'd like to keep my modification at each code r...

stanypub by Associate
  • 1897 Views
  • 2 replies
  • 0 kudos

STM32F107 ETH DMA hangs on reset

Posted on October 10, 2016 at 18:29Hi, I generated project in CubeMX, and I can't run ETH. Connections to PHY are fine. My program run on line 215 in file stm32f1xx_hal_eth.c whitch is:while (((heth->Instance)->DMABMR & ETH_DMABMR_SR) != (uint32_t)R...

jakub2 by Associate
  • 1301 Views
  • 1 replies
  • 0 kudos

Compile error in stm32f4xx_hal_i2c.c.

Posted on October 09, 2016 at 09:45I'm getting a basic compile error in stm32f4xx_hal_i2c.c. The header on the file says:   * @file    stm32f4xx_hal_i2c.c   * @author  MCD Application Team   * @version V1.5.1   * @date    01-July-2016 I see: HAL_Sta...

stm32f4 dongle 3g/gsm

Posted on October 07, 2016 at 15:16Hello everybody,before I start I would like to thank you and I apologize for my bad English.good, I want to use a dongle 3G/GSM (USB) with STM32f407 (the card discovery), and I do not know or begins1- I use USB OTG...

rafik by Associate II
  • 693 Views
  • 0 replies
  • 0 kudos

STM32L476 Discovery CDC configuration change

Posted on October 05, 2016 at 12:48Hi all,I'm working on a USB CDC demo from cubel4 family under the STM32L476G_EVAL board.I port the example to work with the STM32L476_VG_Discovery changing the PIN.The example configure the board to receive from a ...

scash9 by Associate
  • 1104 Views
  • 1 replies
  • 0 kudos