STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hardfault Systeminit STM32Cube_FW_F0_V1.2.0

Posted on February 02, 2015 at 10:18Hi,Using the STM32F0308-DISCO eval board and the STM32Cube_FW_F0_V1.2.0I am compliling using eclipse and GCC ARM Sourcery tools with openOCD debugger.The GPIO_IOToggle example compiles, loads and runs in the debug...

COM port disconnect from USB way to know it STM32F205

Posted on November 17, 2014 at 07:29I use today the USB OTG with ST example stm32_vcp_1.3.1.I want to know if there a way to know that a connection I made with teh PC by openning COM port close.I use today the function  DCD_OTG_ISR(USB_OTG_CORE_HAND...

Barbie by Associate II
  • 629 Views
  • 2 replies
  • 0 kudos

how send NULL string with lwip?

Posted on January 28, 2015 at 23:28i can send string with lwip.how send NULL string with lwip sprintf(BUF,''(%c%c%c%c'',len/256,len%256,Cmd/256,Cmd%256);  strncat(&BUF[5],buf,len);   strncat(&BUF[5+len],'')'',1);  tcp_write(TcpPCB,BUF,BufLen+6,1); i...

h_kabiri by Associate II
  • 1504 Views
  • 8 replies
  • 0 kudos

STM32L151 Slow USB speed

Posted on November 27, 2014 at 15:12Hello all,I have a quick question regarding the USB FS speed on STm32L151.I managed to modify the sample code for USB VCP and get the USB running. I'm streaming my data to the PC succesfully.The question is follow...

srdjan by Associate II
  • 430 Views
  • 1 replies
  • 0 kudos

CAN application using HAL Library

Posted on January 26, 2015 at 16:01Hello there, I am new to STM32 but I have some expirience with AVR8 and 32. I am trying to make a simple demo program using stm32f4discovery board that would allow me to send and receive data on CAN1 channel. For t...

Sd card damage after writing data[SOLVED]

Posted on January 20, 2015 at 14:41I am getting a very annoying problem where my SD cards are becoming corrupted after recording data through a custom PCB. I'm using the SDIO driver (fixed for 4GB), that clive has made available in the forum, for in...

felipe2 by Associate III
  • 3376 Views
  • 8 replies
  • 1 kudos