STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Standby mode with RTC

Posted on April 11, 2017 at 14:32HelloI would like to perform a standby mode at the start of my microcontroller and return to normal mode with RTC Alarm A. But for now I can't find a reliable documentation or example to get a result. I work with Cub...

ibrahim by Associate II
  • 1751 Views
  • 2 replies
  • 0 kudos

Resolved! USB CDC device receive fails on transmit

Posted on March 31, 2017 at 23:39I am using the USB CDC library on a STM32F746 as created with CubeMX and have run into a problem when the MCU transmits at the same time that it is receiving over USB.  I had a PC bursting data to the MCU.  The data ...

JD1800 by Associate II
  • 4312 Views
  • 3 replies
  • 0 kudos

RunTime DFU with USB in STM32L4

Posted on April 10, 2017 at 12:28Good mornign,I'm working in my application that is based on STM32L475 device.I'm able to flash my device by using the Dfulse Demo software and setting Boot0 to 1 when applying power to device. But I would like to imp...

How to convert .wav audio to C code?

Posted on April 09, 2017 at 08:14Hi, I'm using Audio_playback_and_record example in STM32F4 Discovery in internal flash mode. But how can I change the audio_sample.c? How can I convert .wav audio to C code?#audio

Karim by Associate II
  • 1598 Views
  • 1 replies
  • 0 kudos

Cube 4.20 bug - Clock initialization

Posted on March 16, 2017 at 10:54 I found a bug in the new Cube Version. At line 1 internal oscillator is enabled although it is not used, in fact it is not actived: RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTY...

AndreaC by Associate III
  • 2793 Views
  • 6 replies
  • 0 kudos

STM32L433 USB VCP Problem

Posted on April 05, 2017 at 20:36Good evening everyone,I'm trying to use the L433 USB as VCP using HAL Drivers, to receive data from PC and transmit the response to the PC.I'm following the STM32L452RE example 'Standalone CDC' from the CubeMX exampl...

FreeRTOS Mutex example ?

Posted on April 03, 2017 at 00:53 Everyone, Does anyone know where I can find a simple example for FreeRTOS on Mutex ? I want to do two task but the first task never finishes and jump already to the second one because of the systick, how can ...

antonius by Senior
  • 14123 Views
  • 21 replies
  • 0 kudos

There is a wrong comment in stm32f1xx_hal_dma.c

Posted on April 05, 2017 at 07:49static void DMA_SetConfig(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength){/* Configure DMA Channel data length */hdma->Instance->CNDTR = DataLength;/* Peripheral to Memory */if...