cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 using callbacks to retrive data from USB CDC VCP

Mohammad A
Senior
Posted on April 11, 2017 at 07:41

I have generated a project for USB CDC VCP using CubeMX and HAL and now I am trying to figure out how I can implement these two weak functions:

void HAL_PCD_DataInStageCallback(PCD_HandleTypeDef *hpcd, uint8_t epnum) 
void HAL_PCD_DataOutStageCallback(PCD_HandleTypeDef *hpcd, uint8_t epnum)�?�?

These fuctions will be called inside HAL_PCD_IRQHandler. What I want to do is place some code inside them so I can retrive received data from host and also find out about end of transaction.

I have seen that CubeMX has reimplemented these weak functions inside usbd_conf.c like this:

/**
 * @brief Data Out stage callback.
 * @param hpcd: PCD handle
 * @param epnum: Endpoint Number
 * @retval None
 */
void HAL_PCD_DataOutStageCallback(PCD_HandleTypeDef *hpcd, uint8_t epnum)
{
 USBD_LL_DataOutStage((USBD_HandleTypeDef*)hpcd->pData, epnum, hpcd->OUT_ep[epnum].xfer_buff);
}
/**
 * @brief Data In stage callback..
 * @param hpcd: PCD handle
 * @param epnum: Endpoint Number
 * @retval None
 */
void HAL_PCD_DataInStageCallback(PCD_HandleTypeDef *hpcd, uint8_t epnum)
{
 USBD_LL_DataInStage((USBD_HandleTypeDef*)hpcd->pData, epnum, hpcd->IN_ep[epnum].xfer_buff);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

I am wondered to know what do these two functions (USBD_LL_DataOutStage and USBD_LL_DataInStage) do? And how I can edit them to achieve my goal.

#hal #usb #cdc
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0