STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401RC fatfs internal flash

Posted on May 11, 2017 at 09:45Hi guys,     These days, I am doing some test on the internal flash with fatfs on stm32f401rc. And now, I know there is many sample with the SD card, and also in the cubemx, I find the example with SD card and USB devi...

0690X00000606t7QAA.png 0690X00000606w1QAA.png
cable gu by Associate II
  • 1186 Views
  • 1 replies
  • 0 kudos

STM32F4 Discovery Ethernet

Posted on November 17, 2011 at 13:13hello friends Can any body guide me on how can i use the ethernet module of stm32f407 on discovery kit? do i need something extra? #stm32f4-discovery #ethernet #lwip

najeeeb by Associate
  • 10361 Views
  • 20 replies
  • 0 kudos

STM32F4 USB FS and PA8 as output not working

Posted on May 17, 2017 at 15:52Hi,I'm using the STM32F446ZE.I'm using PA11 and PA12 for USB FS DM and DP, but I don't need PA8 as SOF, I need it as a simple output.USB is runing fine only if PA8 = 0 !If I set PA8 output to 1, the USB disconnects.It ...

Kuikui by Associate III
  • 9322 Views
  • 27 replies
  • 0 kudos

STM32F303VB: USB related queries

Posted on June 13, 2017 at 14:59Hi,We are using STM32F303VB on our custom hardware. We plan to use the STM32 as a USB device talking to a PC (USB Host).(I'm using STM32CubeMX (STM32Cube_FW_F3_V1.8.0) to generate project for AC6 System Workbench.)I h...

Prasant J by Associate III
  • 766 Views
  • 0 replies
  • 0 kudos

simple USB circuit

Posted on June 03, 2017 at 18:53hello,I would like to have some clarification about the USB circuit needed for the stm32f103 (and similar), I am making a simple development board just to start learning this MCUThis is taked from the maple mini https...

0690X00000607DzQAI.png