STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL CAN recovery example

Posted on August 05, 2017 at 20:12Is there a good example on how to restart CAN after it turns off due to too-many bus errors?I have a CAN bus with a lot traffic and its quite normal for a particuar device to fail on re-transmit a large number of ti...

DJC by Senior
  • 3102 Views
  • 3 replies
  • 3 kudos

Start USART Bootloader on STM32F070 device does not work

Posted on May 22, 2016 at 10:50Hi all,i am using a Nucleo board ''NUCLEO F070RB'' and i want to start the UART Bootloader. Unfortunately the bootloader doesn�t send the Ack  byte (0x79) after activation.My procedure to start the bootloader:- connect...

tj by Associate II
  • 6875 Views
  • 18 replies
  • 0 kudos

USB cant send multiple messages

Posted on August 26, 2017 at 08:58USB cant send multiple messages though I gave delay.How many messages I want to send It only sends one.Where do I mistake?Probably your code also has an error because I have not changed anything.#usb

0690X000006042GQAQ.jpg

STM32F072R8 Bootloader jumping with USART3

Posted on August 24, 2017 at 17:18   I am trying to utilizes the 'Flash Loader Demonstrator by STM' to download new firmware onto the STM32F072R8 chip and I will not be able to use the pin  BOOT0  on my board. The idea is to use the main program to ...

Raj Patel by Associate II
  • 2964 Views
  • 8 replies
  • 0 kudos

Resolved! STM32F0 Scan ADC Polling Sequence

Posted on April 11, 2017 at 09:41 Good Day Please help me understand if I am using the Polling Mode correctly for the ADC. I have not gone through the trouble of setting up DMA or Interrupts because these functions will hardly ever be used in ...

abotha by Associate III
  • 3416 Views
  • 6 replies
  • 0 kudos

Incorrect operation HAL_SPI_Transmit?

Posted on August 23, 2017 at 15:27Hello! I work under STM32F051. When working with the HAL_SPI_Transmit and HAL_SPI_TransmitReceive functions, one thing happened: when data is transferred in SPI_DIRECTION_2LINES mode, the data is also received in th...

Runtime DFU application in STM32L4 series

Posted on December 08, 2016 at 14:07 Hello Everyone, I need DFU application which can load the new firmware at run time. I want to implement DFU in stm32l476G-Eval board, tried with DFU bootloader method (Connecting Boot0 to VCC) it is working ...

VDDUSB connection

Posted on August 22, 2017 at 15:07Hello there,I have a question regarding VDDUSB connection in STM32L452 MCU. Should it be applied all the time, or only when the USB cable is being connected? I was wondering either it is possible to apply it from th...