STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB communication at 50Mbps using STM32

Posted on December 13, 2016 at 09:18Hi all,I would like to implement USB communication at 50Mbps using STM32 as a device- based on ST's existing example code.I would like to understand if this is possible to achieve using the standard example code a...

udilevy by Associate II
  • 524 Views
  • 0 replies
  • 0 kudos

STM32F4 HAL Driver Callbacks

Posted on December 11, 2016 at 03:15Hi.I am developing for an STM32F4. I'm using STM32CubeMX and System Workbench for STM32. I'm using FreeRTOS. I would like to know how I should, and should not, be using the STM32F4 HAL Driver callbacks. As an exam...

STM32F746-DISCO SD card USB MSP

Posted on December 09, 2016 at 21:31Hi,I'm trying to read SD card using Mass Storage Protocol via STM32F746-DISCO board. I found example in Applications\USB_Device\MSC_Standalone which does exaclty what I need. However the read/write speed is bad. I...

karol1dw by Associate
  • 553 Views
  • 0 replies
  • 0 kudos

STM32F7 Ethernet operation TE vs. ETH_TX_EN

Posted on December 08, 2016 at 22:38Hi all, I'm working with Ethernet on an STM32F745IETx and with a project configured using STM32CubeMX. We're using an RMII interface to a chip that supports three Ethernet ports. I've tested pass through between t...

hbarta2 by Associate III
  • 610 Views
  • 2 replies
  • 0 kudos

examples in Cube

Posted on November 27, 2016 at 03:51 Anyone figure out how to run the examples downloaded with Cube ? I am using the f0, r8 chip with the nucleo board. I have been programming using bare metal (registers) and some spl to learn about the chip. No pr...