STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LwIP UDP Define has no reference

Posted on June 22, 2017 at 17:28Hello fellow Ethernet explorersI am currently trying to make a UDP connection between a stm32f4 discovery board and a pc.I have already made an example work and I am now trying to replicate the result but with a progr...

andy b by Senior
  • 1624 Views
  • 4 replies
  • 0 kudos

how to implement a high prio timer interrupt in parallel or as freertos thread with ~100 ns accuracy

Posted on June 16, 2017 at 22:43Hi basically I am using freertos in my project and I need a highest prio timer interrupt driven task which needs to be executed in a granularity of 100 ns. (every n* 100 nsec like 100ns, 1500ns,....)In Cube MX I sat u...

Boot loader flashing fails (occasionally)

Posted on June 06, 2017 at 14:12I have an STM32F103 that I'm re-flashing remotely using a different MCU through its UART port (using the boot loader). It works perfectly fine, I have multiple devices that have been successfully flashed with the righ...

STM32F4/7 TWO FS USB

Posted on March 10, 2017 at 15:39Hello ; I tried to read the reference manual but still not clear ; is it possible to use  USB FS ( GPIOA ) and USB_ hs ( FS mode) ( GPIOB) at same time in host mode ?in our applicstion we need two host USB to communi...

STM32F401RC fatfs internal flash

Posted on May 11, 2017 at 09:45Hi guys,     These days, I am doing some test on the internal flash with fatfs on stm32f401rc. And now, I know there is many sample with the SD card, and also in the cubemx, I find the example with SD card and USB devi...

0690X00000606t7QAA.png 0690X00000606w1QAA.png
cable gu by Associate II
  • 653 Views
  • 1 replies
  • 0 kudos

STM32F4 Discovery Ethernet

Posted on November 17, 2011 at 13:13hello friends Can any body guide me on how can i use the ethernet module of stm32f407 on discovery kit? do i need something extra? #stm32f4-discovery #ethernet #lwip

najeeeb by Associate
  • 6081 Views
  • 20 replies
  • 0 kudos