STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why HAL_UART_RxCpltCallback doesn't work?

I try to use uart interrupt for communicate with hyperterminal. It seems that HAL_UART_RxCpltCallback doen't work. I made the configuration in STM CUBEMx . It send the first burst throught interrupt routine and receive only one time the aRxBuffer. Th...

EnricoT by Associate
  • 679 Views
  • 0 replies
  • 0 kudos

Firmware Upgradation through USB

we are using STM32F407 controller in our project. In this we have taken an option of firmware upgradation through USB. Everything is fine and works good but for some controllers USB is recognising directly and for some it is recognising if there is o...

saiteja by Associate II
  • 1620 Views
  • 4 replies
  • 0 kudos

stm32F4 BACKUP SRAM and USB HID conflict

Posted on November 25, 2014 at 15:37Hi, usb hid works form me great on discovery f4 but I have a problem with saving to backup sram and backup rtc after USB initialization. I would like to create a program, which is waiting for character from the US...

jakub by Associate
  • 5266 Views
  • 13 replies
  • 0 kudos

UART hal RX interrupt modification

My scenario I have a master controller keep sending 30Bytes of data with every 500ms..Issue when use to my slave controller is :HAL_UART_Receive_IT(&huart1, varPtr, 20);the packet might not be received properly as the slave is hot swapped.. it can be...

Boot STM32H7 after power up

According to PM0253 "Programming Manual" after power up the the vector table is located at address 0x0000000. This memory is RAM memory (ITCMRAM) so how the boot can run from it if it just powered up? ​There is no memory address in it...In other CPU ...

Yood by Associate II
  • 2120 Views
  • 4 replies
  • 0 kudos

STM32F7-FFS-FreeRTOS Hard Fault

I am working with a sample project for the stm32F746G. Testing on the Discovery Board. I am using VisualGDB. The project is USB Device | MSC Host RTOS. After importing the project and tweaking a few things It did run. (However, all of these projects ...

Jona by Associate III
  • 1209 Views
  • 1 replies
  • 0 kudos