STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use F746NG-DISCO and USB OTG_HS

HelloI want to send 45 Mbyte/sec data from the discovery board to PC . So I need to use usb high-speed protocol (CDC). But PC doesn't find the device (I've checked it via the device manager). I used the CubeMX for code generation.What I simply did is...

Cevdet by Associate III
  • 3785 Views
  • 6 replies
  • 0 kudos

How set USB-CDC (Virtual Com Port) baudrate

Posted on July 07, 2016 at 18:47Hello, I'd like to transfer some data via USB FS with Virtual Com Port (STM32F3) Seems that baudrate is fixed to 115200 bps. It is possible to increase this value? How? Thank you very much #stm32 #cdc #baudrate #vc...

lrosadev by Associate II
  • 9178 Views
  • 4 replies
  • 0 kudos

STM32 Composite Device

Hi there,are there good Tutorials, Examples or Explanations how to implement a composite device example? Like using cdc+hid or cdc+hid+msc?I appreciate every help because i can't find any useful information on that.Thanks in advance

arduo by Senior
  • 745 Views
  • 0 replies
  • 0 kudos

FreeRTOS - timing weird-ness

Hi All,I'm building up my understanding of using FreeRTOS, and what I've setup is a Nucleo-F103RB connected to a logic analyser. The plan here is to have a few tasks setup with RTOS to toggle LEDs at varies rates and timings and then check how this a...

stm32cubeMx stm32f2 USB_OTG_HS warning

Posted on April 27, 2015 at 07:11when I select USB_OTG_HS->extern phy->device only peripherals, I got warning:These IPs still have some not configured or wrong parameter values?[Clock]Do you still want to generate code.what does this exactly mean? a...

Buffer size for USB on the STM32L4 device.

Hi I am using the stm32L433 device and want to use the USB port for communication. I am planning to use it as a CDC class, and to start of with using the cube (then modify it to use registers only). I have read some place that it requires a large bu...

slow boot from Bank2 STM32L4

Posted on March 29, 2017 at 17:05Hi everyone,I want to use the dualbank boot and upgrade mechanism as described in AN4767 with my STM32L476.Toggling the booting bank with the BFB2 flag works fine.Unfortunately, I observed that the booting process ta...

Micha K by Associate
  • 967 Views
  • 1 replies
  • 0 kudos