STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why STM32H743ZI DFU bootloader does not come up?

Hell ST community!I have made a board with an STM32H743ZI MCU on it. It has connections to pins where serveral USART peripherals sit (without pull-ups) and uses USB FS on PA9 to PA12.My problem is that the DFU bootloader does not show up via USB. If ...

martin.k by Associate II
  • 4334 Views
  • 8 replies
  • 0 kudos

Resolved! Canbus Filter Matching Index

Hi, I'm fairly new to arm platform. I'm trying to communicate between 2 MCU via Canbus. with the latest HAL Library I set up 4 filters (2 for each fifo) id mask type , 32Bit. I am receiving my messages from correct fifos. what I cant get is filter ...

e-zeki by Associate III
  • 5159 Views
  • 10 replies
  • 0 kudos

Resolved! Warn : no flash bank found for address 0

Hello, I am getting acquainted with FreeRTOS using HAL Libraries. For that I have created two tasks, Task 1 and Task 2 and am simply printing "Task 1" and "Task 2" over a UART. If I build the project from scratch, then I get the text, data, bss sizes...

Hello everyone, I used a bootloader for Stm32f1xx, but if I use hal_delay after the jump function, the microcontroller stops working. I'm waiting for your help.

if (HAL_GPIO_ReadPin(button_GPIO_Port,button_Pin)==1) //mypushbutton==1 {   /* If Key is pressed */  /* Execute the IAP driver in order to re-program the Flash */  printf("\r\n\r\n");  Main_Menu(); }// /* Keep the user application running */ else { ...