STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there a way to make HAL_ETH_GetReceivedFrame wait for a frame to be received ? Also can the frame be filtered by ethertype ?

I am trying to receive raw ethernet frames on my STM32F746G and i want to wait for their arrival and filter them by etherType.In the reference manual only filtering by Source or Destination address is possible and i don't seem to understand where to ...

khaaal by Associate II
  • 2025 Views
  • 3 replies
  • 0 kudos

HAL_UART_DMA_Receive problem

Hi guys.I have a problem with this hal function.The problem is that every time I use this function the first byte received is not what I transfer to it.For example when I send AT (ESP8266 AT command) to the module it must return AT OK,but every time(...

sending data problem LWIP without RTOS

Hello,I am trying to send data periodically as a client in MCU.I am using program called SocketTest v 3.0.0 from PC.Connection is OK but I can't see other values.These are my codes.---------------------in main.c------------------------   #include "m...

Zek_De by Senior
  • 1855 Views
  • 6 replies
  • 0 kudos

MCU freezes when starting ADC in DMA mode

Hello, i want to start an ADC in DMA Mode, but everytime i run HAL_ADC_Start_DMA the MCU stops.Here is the section of my code where it happens: if(newpwmperiod == 1 && adc_dma_status == 0){ HAL_UART_Transmit(&huart2, test, 4, HAL_MAX_DELAY); ...

AKons by Associate
  • 1026 Views
  • 0 replies
  • 0 kudos

Resolved! The Speed of GPIO is much lower than expected.

I am using stm32f205ret. I want to toggle as fast as possible. According to the data sheet i should be able to do it at 60 MHZ. I use cubeMX to initialize my code. I basically set all clocks to max. I set one pin (gpio port C pin 5) as GPIO_OUTPUT. I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.