2019-09-13 3:24 AM
I am using stm32f205ret. I want to toggle as fast as possible. According to the data sheet i should be able to do it at 60 MHZ. I use cubeMX to initialize my code. I basically set all clocks to max. I set one pin (gpio port C pin 5) as GPIO_OUTPUT. I configure the speed of the port to be high in cubeMX. And keep toggling it in a while(1) loop.I cannot go beyond 1MHZ.
I would be really nice if someone can tell what I am missing. I have attached the code for clock setup and gpio setting:
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5, GPIO_PIN_RESET);
/*Configure GPIO pin : PC5 */
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 13;
RCC_OscInitStruct.PLL.PLLN = 195;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2019-09-13 4:12 AM
This comes up every now and again, particularly with those who are used to PICs or other "small" microcontrollers.
There are a few issues.
Most people go to 32-bit microcontrollers for the amazing amount of processing that's possible. Not for fast I/O.
Hope this helps,
Danish
2019-09-13 4:12 AM
This comes up every now and again, particularly with those who are used to PICs or other "small" microcontrollers.
There are a few issues.
Most people go to 32-bit microcontrollers for the amazing amount of processing that's possible. Not for fast I/O.
Hope this helps,
Danish
2019-09-13 4:17 AM
In addition to what Danish wrote, for most cases of fast I/O requirements you can use the timers, they are very flexible. In some other cases (like fast parallel I/O) you can use the FMC/FSMC peripherals.
2019-09-13 5:02 AM
>>I cannot go beyond 1MHZ.
You're loop, which you fail to show, must be very inefficient. Look at the assembler code generated.
2019-09-13 12:10 PM
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.