STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F723 USB Device MSC with internal flash

Hi!I am using stm32f723 to implement usb device mass storage.I try to mass storage using an internal flash, but I get a message that the formatting is not complete.I have developed it by referring to the link below, and I have confirmed the same valu...

SKoh.12 by Associate II
  • 1779 Views
  • 4 replies
  • 0 kudos

STM32L476RG FreeRTOS multithread issue

Hi Experts,I am using STM32L476G MPU, (which sensortile board) and used the following SDK & sensortile BLE example.~\STSW-STLKT01_V1.3.1\Projects\SensorTile\Applications\BLE_SampleAppAdded FreeRTOS support for multithread in my BLE example.~\STSW-STL...

Update only one section with code/functions

Hello,I was wondering if it was allways necassary to implement a bootloader and load the entire app to flash. Would it be possible to place some frequently updated functions in an own section (with variables stored in own section in Ram) and only upd...

machinist by Associate III
  • 794 Views
  • 3 replies
  • 0 kudos

STM32L433 doesn't generate the UART_IT_IDLE Interrupt

Hello, everyoneI have an STM32L433 that must communicate with other device via UART.When I activate xfer with commands:__HAL_UART_ENABLE_IT(uartHandle, UART_IT_IDLE); HAL_UART_Receive_DMA(uartHandle, &rxBuffer[0], rxBufferSize);I expect that when o...

Uhv by Associate II
  • 557 Views
  • 0 replies
  • 1 kudos

Problem with USB CDC on STM32F4-Discovery

Hello.I'm working with STM32F4-Discovery. I use USB CDC VCP for transmit data from ADC to PC and receive command from PC to change timer period. Program is written with HAL drivers, with help of CubeMX. Problem is with receiving command, because some...

leonsk by Associate II
  • 461 Views
  • 0 replies
  • 0 kudos