STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ThreadX api documentation/summary?

Hi all,Is there documentation that shows the ThreadX functions with an explanation of the function's parameter? and which are mandatory and which optional?This is an example of a simple function call generated by cubeMX: /* Create tx first thread. *...

Rodo by Senior
  • 1218 Views
  • 2 replies
  • 0 kudos

Resolved! zephyr stm32u5g9j-dk2 adc not function

Hello, I am using the Zephyr operating system with the STM32U5G9J-DK2 hardware. I intend to collect voltage data using the ADC, but so far, no progress has been made. Here are the steps I have taken: I used the zephyr\samples\drivers\adc\adc_sequenc...

devin-hu by Associate II
  • 699 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 - FileX and MSC - Windows read wrong data

Hi, I'm on a applicaiton involving USBX MSC and FileX. The final memory for the application is a NOR flash so I also use LevelX.Acutally, I'm working on a nucleo-U575ZI-Q without NOR flash so I use NOR Simulator on LevelX.My problem is that a file cr...

Dams_0-1760544703605.png
Dams by Associate III
  • 2799 Views
  • 20 replies
  • 1 kudos

NUCLEO-H563ZI Factory Demo Image

Hi. How can I build the Demo FW initially running on NUCLEO-H563ZI ?The is a number of projects in Cube under STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI but it is not clear which one is the factory used to initially program the board. Thanks.  

dimax by Senior
  • 670 Views
  • 3 replies
  • 0 kudos