STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fluctuation in the high voltage level

Posted on June 26, 2018 at 09:00In STM32F411 Discovery board, The STlink was not able to program the on board STM32f411, so i have usedSTLink /v2 external module to load the program into MCU. I have also applied the target voltage 3.3V to the board ...

Is it mandatory to cut off the Nucleo board in order to use PA13 and PA14 to program with ST-Link/v2?

Posted on June 25, 2018 at 18:59Hi everyone,I play with a Nucleo-F767ZI, using the ST-Link part provided on the PCB.I would like to use a ST-Link/v2 to program my MCU.I was wondering, whether it is possible to power my MCU (without USB PWR) and use ...

0690X0000060BrtQAE.png 0690X0000060BnnQAE.png
ced seg by Associate II
  • 1876 Views
  • 2 replies
  • 0 kudos