STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-F767ZI No ST-Link detected.

So I have a Nucleo-F767ZI development board and I wanted to try out some applications on it but unfortunately once I try opening the debugger it gives me a "no st-link detected" error message. I have a Mac running running the latest version of macOS....

Is there a possibility to read program counter via ST-Link or J-Link without causing a reset on STM32F103 devices with RDP active?

On a serial product after a firmware update, there are some sporadic cases, where we get a hang up situation. It would be very helpful to know where exactly the program is stuck. According to ES0346 Rev. 6 chapter 2.8 it is possible to access progra...

stst9185 by Associate III
  • 6746 Views
  • 13 replies
  • 0 kudos

Incorrect voltage on input pin of STM32L4Q5CG when pulled-up to supply voltage via external resistor

Hello All,I have the following setup:Stand-alone STM32L4Q5CG on 48-pin breakout board with coupling caps installedPB11 tied to 3.3V via external 4.7K pull-up resistorPB9 tied to 3.3V via external 4.7K pull-up resistorSTM32CubeMx rev. 6.0.1 Firmware p...

ebce3 by Associate II
  • 2537 Views
  • 6 replies
  • 0 kudos

Resolved! Read and write using ST-Link V2

Hi everyone,I do have 2 PCB boards based on STM32F030F4P6 MCU, the two PCBs have the same hardware and connection with other components, I read the first MCU's code using ST-LInk V2 -using SWD- and saved the .hex file to my PC then I wanted to re-pro...

AKh.2 by Associate II
  • 11885 Views
  • 12 replies
  • 0 kudos

LDO for STM32L433?

Hello, I would like to know what LDO regulator you recommend to use in my development, it uses a 7.2V Lithium battery pack. The application uses 5 GPIO's (4 output, 1 input), 1 I2C, 2 USART, 1 LPUART.

AStol.2 by Associate II
  • 2036 Views
  • 4 replies
  • 0 kudos

Resolved! Location of STM32H747I-DISCO BOOT0 pin

I have a board that is STM32H747I-DISCO which was bricked due to the power supply settings improperly set (Set to LDO when it shouldve been SMPS) in the code.The documentation say to boot with BOOT0 pin set in order to restore the working image, I do...

xlpaudst by Associate
  • 3677 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F030R8T6 pin to pin alternative product

Hello Community. STM32F030R8T6 seems to be unavailable. This is a huge problem. Does it exist a pin to pin an alternative (also on other families (STM32F1, F2, f3...).STM32F030RC is NOT a solution since it appears not to be available too. In any case...

raffin by Associate III
  • 2018 Views
  • 3 replies
  • 0 kudos