Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP and int

My customer installed some sites with cards with S2-LP (one central board and one remote).On a particular location the S2-LP crashes. Now I'm searching the problem but while I'm searching I would like that the customer resets the S2-LP (not the entir...

Capture d’écran 2023-06-21 175501.png
PCu1 by Senior
  • 884 Views
  • 0 replies
  • 0 kudos

BlueNRG-2 IRQ problem

Hi,I have a custom PCB based on STM32L4R9 with a SPI interface to BlueNRG-2 flashed with DTM SPI (2.1f stack). I use X-CUBE-BLE2.I'm able to communicate with the module such as retrieve firmware details, start and stop tones. The problem I'm seeing i...

CBras by Associate II
  • 948 Views
  • 0 replies
  • 0 kudos

STHV series evaluation board and chips

Hi,I notice that the STHV series chips have T/R switch in it, but I wonder if the evaluation board can receive the echo signals? Then, if I want to develop a PCB board with STHV series chips, do I need to add a waveform generator before STHV chips?...

SWang.18 by Associate
  • 966 Views
  • 0 replies
  • 0 kudos

How to bootstrap profile to eSIM chip

Hello,I'm from Viet Nam,I am currently working on a project to use eSIMs for electronic meters.Can you show me how to bootstrap VNPT's profile to your eSIM chip? (VNPT is a major telecommunications corporation in Vietnam)Best Regard!

TChu.5 by Associate
  • 1386 Views
  • 1 replies
  • 1 kudos

BLE_STATUS_TIMEOUT with terminate_gap_procedure

Hi everyone,I am developing an IOT solution using the BLUENRG-M0 from ST.I am coding in C and I use a custom board with SPI communication between the BLUENRG and my MSP430F5255 from T.I . I am using the ACI API to transmit commands to the BLE module....

GBara.3 by Associate II
  • 3684 Views
  • 11 replies
  • 0 kudos

I purchased the STUSB4500QTR and actually operated it. After assembling the electronic board, I dumped the default contents of the register and it became as shown in [1A] below. Next, when I purchased parts from a new lot during mass production and assemb

*********************************************************************************(Contents of register [1A])0xC0: 0x00 0x00 0xB0 0xAA 0x00 0x45 0x00 0x00 0xC8: 0x10 0x40 0x9C 0x1C 0xF0 0x01 0x00 0xDF 0xD0: 0x02 0x40 0x0F 0x00 0x32 0x00 0xFC 0xF1 0xD8...

ODais.1 by Associate
  • 1335 Views
  • 0 replies
  • 0 kudos

Hi I am implementing a nrf24l01 driver with the use of stm32F4 the SPI transmit and receive works with the polling method yet not with DMA method.I already configured the DMA on cube mx and IAR WORKBENCH this is the code part i put the dma as cmnt

//3. Read single byte from a registeruint8_t NRF24_read_register(uint8_t reg){   uint8_t spiBuf[3];   uint8_t retData;   //Put CSN low   NRF24_csn(0);   //Transmit register address   spiBuf[0] = reg&0x1F;   HAL_SPI_Transmit(&nrf24_hspi, spiBuf, 1, 10...

atoua.1 by Associate
  • 1426 Views
  • 0 replies
  • 0 kudos