Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Have you seen the source code to the MFX?

Hi All,Some of the grander Evaluation/Discovery boards use an STM32L152 as a slave Multi Function eXpander with an I2C interface. It's pre-programmed with firmware that provides access to some of the peripherals on the board.As it happens, I'm about ...

DOsbo by Senior
  • 1744 Views
  • 1 replies
  • 0 kudos

Help with sensortile.box, STM32duinoBLE, and GATT

Help, anyone! What am I doing wrong??Below is the entirety of the skeleton code that I have written to add a GATT service to the basic sensortile.box. The issue I have is I only get two generic services:00001801-0000-1000-8000-00805f9b34fb (Handle: 1...

GEmel.1 by Associate II
  • 1891 Views
  • 1 replies
  • 0 kudos

BLUENRG-2

Hello ST-CommunityI have a little problem with bluenrg-2m, I'm handling the the user event process in 100ms RTOS timer call back with stmn32f446.The problem is when I send a file using mobile app call bluetooth terminal, It become too slow !1kbyte pe...

MOhamed_Mehery_0-1687498597311.png

S2-LP and int

My customer installed some sites with cards with S2-LP (one central board and one remote).On a particular location the S2-LP crashes. Now I'm searching the problem but while I'm searching I would like that the customer resets the S2-LP (not the entir...

Capture d’écran 2023-06-21 175501.png
PCu1 by Senior
  • 868 Views
  • 0 replies
  • 0 kudos

BlueNRG-2 IRQ problem

Hi,I have a custom PCB based on STM32L4R9 with a SPI interface to BlueNRG-2 flashed with DTM SPI (2.1f stack). I use X-CUBE-BLE2.I'm able to communicate with the module such as retrieve firmware details, start and stop tones. The problem I'm seeing i...

CBras by Associate II
  • 933 Views
  • 0 replies
  • 0 kudos