cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-355VC MCU, GPIOs as inputs, interrupts on logic level changes

JPehl.1
Associate III

Hi.

I'm going to use in a design the SiP below, which contains a BlueNRG-355VC MCU inside.

0693W00000Y97GyQAJ.pngI have found the datasheet titled "BlueNRG-LP", and I was reading about the features of the GPIOs.

  • When used as inputs, they can have internally connected pull-down or pull-up resistors.
  • When used as outputs, they can be configured as open-drain or push-pull

My question is about the GPIOs as inputs, are the GPIOs able to generate interrupts on logic level changes at the inputs? All them? No one? Or only a set of GPIOs can do this function? (if yes, I needed to know which of them are able). I did not found this information in the datasheet.

Regards.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0