Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VNH5180A-E

i have buy VNH5180A-E powersso-36 tp pakage some 20pcs but i check measurement not as per datasheetcan you let me knowdimension A /a2 = 2.53 mm  as per our  ( as per datasheet is 2.15-2.47mm)dimension H = 9.91 mm as per our ( as per datasheet is 10.1...

peter_hk by Associate
  • 780 Views
  • 0 replies
  • 0 kudos

Resolved! How are the BLE attribute handle offsets defined?

Where can I find documentation on the BLE attribute handle offsets? I was adapting code from the sensor demo for the BLE NRG 2 and am trying to understand the "aci_gatt_attribute_modified_event" callback. Through observation and experimentation I fou...

BPaik by Senior
  • 5459 Views
  • 11 replies
  • 6 kudos

Resolved! STUSB4500L Logic Voltage

I am wondering what the logic voltage is for the I/O pins on the STUSB4500L. Under operating conditions they are listed as 0V to 4.5V, but the example circuit shows I2C pullup resistors to 3.3V. Is it safe to connect these I/O pins directly to a 3.3V...

S2-LP DK wrong firmware

Hi,I am trying to use S2-LP DK with a Nucleo + S2-LP Shield. I tried several combinations (4 computers (Windows 10), 6 Nucleo Boards (STML053 and STML152) and 4 S2-LP shields, S2-LP DK V1.2.0, 1.3.0, 1.3.2), I always get the error that I have the wro...

TKlei.7 by Associate
  • 974 Views
  • 1 replies
  • 0 kudos

Failed to execute MI command: Cannot access memory at address 0xffffffbc

After closing serial port, when i re-open serial port with the updated baud rate, I'm getting an error:  Failed to execute MI command:          -data-disassemble -s 4294967228 -e 4294967330 -- 3          Error message from debugger back end:         ...