Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-1 ble gatt write request

Hi, anyone has an example to share for understand which api function can generate a "gatt write request" ? and how to use it?I'm stuck trying to write from central to pheriperal device, because all writes goes into timeout (pheriperla device disconne...

S2-LP Registers

Hi Everyone,I have some questions regarding the registers of the Sub-1GH transceiver 'S2-LP':1) Which registers (configuration registers) are retained in "standby state", in "sleep_A state" and in "sleep_B sate"? Which registers are not retained, and...

WN by Associate
  • 1192 Views
  • 2 replies
  • 1 kudos

Transmitter and receiver address, s2-lp

Hi, Is it possible to set the address of the transmitter or receiver via S2_LP DK? My project involves sending data via s2-lp between two sets (nucleo-l053r8 with steval-fki868v2), I would like to set one for receive only and the other for read only....

DanielH by Associate
  • 1361 Views
  • 1 replies
  • 0 kudos

Issue when compiling BlueNRG-2 SampleApp

Hi,I'm trying to compile the example called SampleApp using keil uVision as IDE. When the project is created, in the Manage Run-Time Environment, the Startup selector in the Device tab is not selected by default, but I selected it before compiling th...

1.jpg 2.jpg 3.jpg
dsm85 by Associate
  • 1209 Views
  • 1 replies
  • 0 kudos

BlueNRG0 optimizing BLE troughput.

 Hello,I am an engineering student currently working with the BlueNRG-M0 for a student project. My setup consists of a mobile application communicating with embedded firmware through the BlueNRG-M0. However, I'm facing an issue: the throughput is qui...

Reda by Associate
  • 712 Views
  • 0 replies
  • 0 kudos

Optimizing Bluetooth LE

 Hello,I am an engineering student currently working with the BlueNRG-M0 for a student project. My setup consists of a mobile application communicating with embedded firmware through the BlueNRG-M0. However, I'm facing an issue: the throughput is qui...

Reda by Associate
  • 979 Views
  • 0 replies
  • 0 kudos

Configuring STM32U575 for I2C DMA transfer

I am working through a workshop tutorial on how to configure and use GPDMA transfers via the linked list functionality provided in STM32CUBEMX. When setting the linked list runtime configuration a Source Address, Destination Address and Data size are...

ITayl.1 by Associate
  • 2054 Views
  • 0 replies
  • 0 kudos

Resolved! ST4485EB : is it 5V compatible

Hi,The ST4485EB IC mentions that it needs a 3v3 supply. How can we ensure that the A and B lines interoperate with other RS485 devices working at a 5V logic level as the datasheet mentions . Should I just provide 5V supply to this chip so that it int...

Nilav_1-1697524248396.png Nilav_0-1697524168920.png
Nilav by Associate II
  • 2304 Views
  • 4 replies
  • 2 kudos