Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BLUENRG-M2SP SWD connection to STLINK-V3PWR

I currently have a BLUENRG-M2SP connected via SWD to my STLink-V3PWR.The issue is while my flasher can connect to the device it then cannot read the bootloader sector or flash the address memory.Here is the log:16:34:35.247: Waiting device to read bo...

AOdonde by Associate
  • 1857 Views
  • 1 replies
  • 0 kudos

ble disconnection with sleep mode

Have a nice day! I use the Bluenrg-2 chip. As the base project, the Power Consumption Test example is used. The example works fine. But when I use these sources with my bootloader project, a connection problem occurs with BLE_HCI_CONN_FAILED_TO_BE_ES...

rhetti by Associate
  • 865 Views
  • 0 replies
  • 0 kudos

FreeRTOS support for BlueNRG-2?

I am evaluating Keil MDK5 for programming my BlueNRG-2 device. I have found that I cannot create a project from scratch with any RTOS support because the CMSIS driver seems to be lacking the Device.Startup section. Looking in the SDK examples for the...

BBeau by Associate
  • 1897 Views
  • 2 replies
  • 4 kudos

S2LP SMPS1 VOLTAGE PROBLEM

Hello;My Name is FATIHI am using Wireless MBUS water meter scanning using S2LP and STM32L073. While making the PCB design, we applied the reference design value in the x-nucleo-s2868a2_schematic.pdf file exactly. However, although we see VDD voltage ...

FATIH55 by Associate
  • 1001 Views
  • 0 replies
  • 0 kudos