Skip to main content
MSand.1
Associate
February 2, 2024
Question

STEVAL-IDB008V1 - Atollic Truestudio - BLE stack library linking error

Hi,

I ask for the following issue.

I am testing the STEVAL-IDB008V1 board, the BLE RemoteControl example.

I am able to compile the original WiseStudio example project in WiseStudio IDE.

 

THE PROBLEM

I imported the same project from WARM project  in TrueStudio Atollic (9.3 version) according to the importing instruction: I am able to compile the original project files but in the linking phase an error is detected with the libluuemrg1_stack.a library.

Some symbols (related to the the cryptography functions AES......) are not found: a message like

"undefined AES..... isn't used" appears and the link operation (by using arm-atollic-eabi-gcc -o command) finishes without the executable file.

Do you have any suggestion?

Thanks in advance.

Mario

This topic has been closed for replies.