Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Good morning, is there any specific PC software application that can be used with SensorTile kit instead of the Mobile application?

Posted on November 06, 2017 at 11:15Good morning, is there any specific PC software application that can be used with SensorTile kit instead of the Mobile application?My point is to have the same features that can be performed form my labtop instead...

Resolved! Security database management

Posted on March 29, 2017 at 14:26As i understand the programming manual section about bonding on BlueNrg-MS devices, encryption keys are stored in the security database in order to resolve addresses, and encrypt future data connections.This all seem...

aes2 by Associate II
  • 1107 Views
  • 3 replies
  • 0 kudos

BlueNRG-1 Automatic Connection after pairing

Posted on November 02, 2017 at 10:01I have a little problem with BlueNRG-1 chip. I want that the first time I pair my phone with the BlueNRG-1 Testboard.When I switch off bluetooth on my phone (iPhone) and the switch on, I want that my phone connect...

SPWF04S Receiving POST data

Posted on May 17, 2017 at 14:28I am trying to send data from the browser to the module using POST request with output_demo.html. The POST request is limited to 64 bytes, so I cannot send more than 64 bytes with a POST...If I send 65 bytes, the last ...

tabekb by Associate III
  • 3392 Views
  • 15 replies
  • 0 kudos

Use of WHITE_LIST

Posted on November 01, 2017 at 14:00Hello,I am using two bluenrg-1 devices, one of them working as a slave and other working as a master. I would like to know if there is any example I can use where the white_list is used or if anyone can give me so...

jampino by Associate III
  • 1119 Views
  • 3 replies
  • 0 kudos

SPWF01SA file system problem

Posted on September 22, 2017 at 20:40Hello,I use SPWF01SA on IDW01M1 board with stm32l476rg. This setup worked correctly until I updated static httpd filesystem via at+s.httpdfsupdate. File system image has a lot of small files (562), but with total...