Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPBTLE-1S

Posted on October 28, 2017 at 04:28 HELLO, I am using STEVAL-IDB007V1M. I used BlueNRG-1 Navigator with usb connection but they can not recognize the board.However, when I use BlueNRG-2 Navigator they recognized..;;; What should I do?And I flashed ...

SPW04Sx Handshake certificate isue

Posted on April 03, 2018 at 16:27hi,SPWF047Sx, mode AP, FW1.1.0CA, cert, key loading with AT+STLSCERT + datetimecert 2x ecc bundle (prime256V1)client connect to the wifi open.next is AT+S.HTTPGET=192.168.0.2,conf,45061,2,,,config.txt,AT-S.Skip CAAT-...

BlueNRG 2 Bluetooth 5 APIs

Posted on April 04, 2018 at 15:30Hello, I am currently developing a BLE product using BlueNRG2. I see in the datasheet that it is Bluetooth v5 compliant, but in the sample codes for STEVAL-IDB008V1, the APIs do not support Bluetooth v5 features such...

Resolved! SPWF04Sx - STA - Scan Complete:00

Posted on April 04, 2018 at 11:59hi,wifi module SPWF04Sx is configured to STA mode and try to connect to ssid.when ssid is off, wifi module runs (without received cmd AT) and scan:+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete:00is it possible to...

Resolved! SPWF04Sx - FWUPDATE

Posted on April 04, 2018 at 12:15hi,i use AT cmd FWUPDATE to update firmware of wifi module.i see sequence in HandsOn_Draftv3.0AT+S.FWUPDATE=e,192.168.xnextAT+S.RESET -> (Soft_Reset())nextAT+S.FCFGthe FWUPDATE works well (next Soft_Reset()) but i ne...

BlueNRG-MS IRQ

Posted on December 20, 2017 at 10:37 hi. im running a provided example of HID periphProfiles. using STEVAL-IDB005V1D on NXP platform (FRDM-KL43) SPI lines are OK, i can read header from the blueNRG-MS. the thing is IRQ always high. so that ...

asafbit by Associate II
  • 4684 Views
  • 10 replies
  • 0 kudos

SPWF04: Need a pull down at RTS

Posted on March 02, 2018 at 16:34Hi,I changed on my hardware the SPWF01 against a SPWF04 module. I communicate with the module via a STM32. If I use the SPWF04 module, I need a pull down resistor at the SPWF RTS output to get the communication worki...

SPIRIT1 not entering into LOCK state

Posted on April 04, 2018 at 07:02Hi,First of all, sorry for the lengthy message.We are developing a 433 MHz transceiver using SPIRIT1. We were able to run 'SDK_BasicGenreic_A' program provided with the development kit on 'STEVAL-IKR002V3D' daughter-...

SPIRIT1 not entering into LCK

Posted on April 04, 2018 at 06:56Hi,First of all, sorry for the lengthy message.We are developing a 433 MHz transceiver using SPIRIT1. We were able to run 'SDK_BasicGenreic_A' program provided with the development kit on 'STEVAL-IKR002V3D' daughter-...

SPWF04SA datasheet clarifications

Posted on April 03, 2018 at 18:43Hi ST team,Looking over the device datasheet, I had expected to see maximum current consumption at least under TX and RX conditions so I can design power management appropriately.  When this information is missing, I...