Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF04S WiFi on x-Nucleo-IDW04A1

Posted on August 31, 2017 at 18:27MicroPython Scripting Language over SPWF04S document says, module has some built-in python example codes. When I am trying to execute those programs, I am getting errors in those programs.EX:at+s.python=RL_UDP_CL.py...

Download STSW-BLUENRG1-DK

Hi,i can't acces the download link for the development kit in object.The web page redirect me to this https://my.st.com/content/my_st_com/en/products/embedded-software/evaluation-tool-software/stsw-bluenrg1-dk.license=1536969385495.htmlbut there's no...

I cannot get the software for the bluenrg2

I'm trying to download the software for the BlueNRG-2.First there is the option, but when I do the login I cannot see the "get software" button.How could I do? I'm the only one with that problem?Here the link to the page:https://my.st.com/content/my_...

mikmary by Associate II
  • 664 Views
  • 0 replies
  • 0 kudos

Why does BlueNRG-MS, v7.2c, fail on this simple call: aci_gap_start_general_conn_establish_proc_IDB05A1(ACTIVE_SCAN, 192, 96, PUBLIC_ADDR, false); with error code 0x42 #define BLE_STATUS_INVALID_PARAMS (0x42)

BlueNRG-MS is initialized with CONFIG_DATA_MODE_OFFSET as Mode3 or Mode4, still fails.BlueNRG-MS is initialized as GAP_CENTRAL_ROLE_IDB05A1.BlueNRG-MS is not otherwise scanning or advertising or in a connection as a master or a slave.Note that genera...

Please advise me on a basic strategy for adding BlueNRG2 STEVAL-IDB008V2 button press (PUSH1 or PUSH2) recognition to the Android ST BlueMS application.

My application is to have an Android app that detects a single GPIO input (a button press) from the BlueNRG2 module. Is there a more simple starting point than the BlueMS application and it's companion firmware project? I am using Atollic (thank you ...

DCarl by Associate
  • 1161 Views
  • 1 replies
  • 0 kudos

Bluenrg-1 DTM failing

Posted on July 09, 2018 at 14:13Hello all,I am using the DTM for bluenrg-1 I can program the unit and it will work fine but for some reason when the unit is left powered down for a couple of hours and then powered up again some times stops working.D...

jampino by Associate III
  • 1070 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.