User Activity

Hello,I'm working with a custom board mounting the SPSGRF-868 RF 868MHz module, which embeds the SPIRIT1 transceiver.I communicate with it via SPI, using a microcontroller STM32L151.My board is based on the STEVAL-IDS001V4M evaluation board architect...
Hi,I'm using a STEVAL-IDB006V1 and a STEVAL-IDB006V1M as evaluation board. They both mount a BlueNRG-MS.It seems that the first one could work only as a slave and not as a master, even though it should be both. The return code for aci_gap_start_gener...
Hi,I'm using the evaluation board STEVAL-IDS001V4M which has a STM32L152 mounted on.I'm having some trouble on the initialization of the UART2 peripheral.I'm using the ST library contained into the STSW-CONNECT009 packet.To initialize the UART2, I'm ...
I'm trying to download the software for the BlueNRG-2.First there is the option, but when I do the login I cannot see the "get software" button.How could I do? I'm the only one with that problem?Here the link to the page:https://my.st.com/content/my_...