2017-08-31 9:27 AM
MicroPython Scripting Language over SPWF04S document says, module has some built-in python example codes.
When I am trying to execute those programs, I am getting errors in those programs.
EX:
at+s.python=RL_UDP_CL.py
AT-S.Launching script:3:RL_UDP_CL.pyAT-S.OKSTARTrunTraceback (most recent call last): File '3:RL_UDP_CL.py', line 82, in <module> File '3:RL_UDP_CL.py', line 46, in runOSError: 60Its hard to read the script using AT commands, is there any other way to read files from USER FLASH memory? Any USB+MSC option?
I have activated the REPL using AT+s.python command, how can I import python script which is located in SD card.
MicroPython v1.6.2-84-g7f202fb on 2016-07-13; SPWF04Sx with STM32F439
>>> import WLAN_Test.pyTraceback (most recent call last): File '<stdin>', line 1, in <module>ImportError: no module named 'WLAN_Test'>>>Document says, Run offline PC tool to create .img file from .py file and use AT+s.FSUPDATE command to update filesystem, can someone suggest which tool are you using?
Current Micropython Version is 1.9.X, with so many improvements from 1.6, is there anyway that I can update Micropython?
#spwf04sa #x-nucleo-idw04a12018-09-19 3:19 AM
I am having OSError: 60 ,I do not have access to logs of the http server, but I was trying to runs behind a proxy like nginx start getting this. https://www.printererrorrepair.com/epson-printer-support/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.