Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! M48T18-150PC1 Timekeeper

I have a circuit card that uses the M48T18-150PC1 Timekeeper SRAM, and the battery died. I replaced the part but the settings did not save once power was cycled. A second part was used with the same result. Looking at the date stamp, (412) tells me I...

BobW777 by Associate
  • 1664 Views
  • 2 replies
  • 1 kudos

Layer Stackup for BALF-WL-00D3

 My team is trying to design a radio board with the STM32WL and we plan to use the BALF-WL-00D3 in the RF Front End.Based on our requirements, we have decided to go with a 6-layer board and are trying to decide on a stackup (dimensions) for the same....

ST8500 FSK modulation

Hi, I am evaluating to use the ST8500 module as alternative part of the ST7538Q.In our application we have a custom protocol over power line with FSK modulation.Looking all the documentation related to ST8500 I found that it is possible to configure ...

Resolved! BlueNRG-LP maximum advertisement delay.

Hello,When I try to set advertisement delay more than 10000ms, the function aci_gap_set_advertising_configuration return an error 0x82 (BLE_STATUS_INVALID_PARAMS). According to the function declaration, it must be ok:/* .... * @param Primary_Advertis...

jbie by Associate II
  • 4096 Views
  • 7 replies
  • 0 kudos

SPIRIT1 VCO autocalibrate errata

Posted on August 14, 2015 at 19:20So if I want to hop to various frequencies I need to calibrate the VCO each time. That's fine and expected. The SPIRIT1 has a fantastic auto calibration time of only around 50us - one of the features that make it at...

kzkaram by Associate II
  • 2144 Views
  • 3 replies
  • 0 kudos

3-port switch KSZ8863RLL + STM32

Hello! The task is to implement a device with two-port Ethernet. To do this, I developed a circuit, connected the STM32F207 controller to the KSZ8863RLLI Ethernet transceiver via RMII. The controller and the transceiver are connected according to the...

BNiki.1 by Associate
  • 1706 Views
  • 1 replies
  • 0 kudos