2024-05-17 12:05 AM
A cursory search of the internet shows the Zephyr Community decided not to port the BlueNRG-LP for use with the Zephyr Framework/RTOS. The reason they gave (in 2023) was: "not planned". That seemed a bit vague to me.
Though this is likely a question for the Zephyr Community, I wonder if anyone here can answer why there seems to be little appetite for porting the BlueNRG-LP to Zephyr? I considered undertaking this effort myself but wasn't sure if there is a reason bigger than: "No one has the time or inclination".
I will try to ask the same question of the Zephyr Community if no answer here.
Jeff
2024-05-17 12:10 AM
2025-08-27 5:15 AM
Hello,
may be too late answer, but BlueNRG-LP has been rebranded as STM32WB07 and it is supported by Zephyr now.
Have a look at Nucleo WB07CC — Zephyr Project Documentation
2025-08-27 6:05 AM
Hello Sardo Michele.
Thanks for replying.
Yes, I had moved on to other things but I greatly appreciate you taking time to respond to this question as BlueNRG-LP questions have traditionally received very, very light response traffic in the ST Community.
I do not currently have the rebranded ST WB07CC available to me (only the BlueNRG-LP eval boards currently), but will try once I have the new boards.
Thanks again.
JW