Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Purpose of Smart Card Interface IC.

Hi AllIm relatively new to smart cards. Im wondering what is the purpose of using a Smart card interface IC such as the st8024 other than voltage adjustments? Would it not be easier to interface direct if the the intended smart card is a class B? 3V?

MWolm by Associate
  • 741 Views
  • 0 replies
  • 0 kudos

SPIRIT1 Example Code

I am adding the SPIRIT1 to legacy products that already have a specified MCU.  I have the purchased the full STEVAL-IKR002V3 Eval Kit and two additional daughter boards.  My MCU is able to read/write to the SPIRIT1 registers, but I cannot figure out ...

CKels by Associate
  • 2137 Views
  • 3 replies
  • 0 kudos

Resolved! STUSB1600 (USB Type-C) and USB OTG

I'm trying to understand how I can use a USB Type-C connector together with the STM32MP1 USB OTG peripheral.So obviously I want to use the port in dual role configuration. I want to use the STUSB1600 for that because it takes care of the power source...

arturo182 by Associate II
  • 12339 Views
  • 8 replies
  • 0 kudos

SPBTLE-1S, GPIOs

Hello,I am looking to prototype a project. I will need I2C, SPI and UART.  I2C for some ST sensors/gas gauge, SPI for sd card and UART for RS485.  Is it possible to use SPBTLE-1S, to run both host applications and bluetooth.  Thanks for your help

Sam Ho by Associate II
  • 2016 Views
  • 2 replies
  • 0 kudos

What is the HAL configuration on the STM34F4 discovery for playing wav files converted to 16b hex through the CS43L22 vis I2S?

I'm trying to get the discovery board to play a wav file that I've converted to an array of 16b hex values. So far, I have only been able to output an obnoxious noise. I have tried keeping the registered in the CS43L22 all at default.I have tried con...

TNixo by Associate
  • 782 Views
  • 0 replies
  • 0 kudos

Resolved! [STUSB4500] writing NVM memory on STUSB4500 procedure?

Dear I want to update the NVM memory on the STUSB4500. May I know the procedure of this, I download the STUSB003 SW lib. it not showing how to write NVM. My guessupdate the register call function void nvm_flash(uint8_t Port)reset Am I right?? also wh...

vlee by Associate II
  • 1649 Views
  • 1 replies
  • 1 kudos