Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to compile BLE Mesh project for BlueNRG-2

I am trying to create a BLE mesh project for flashing the BlueNRG 2 board. For this purpose I have downloaded the ST BLE mesh software version 1.07. Then I modified an already working project for the BlueNRG 2 with a working startup and linker file. ...

EBozb by Associate II
  • 1131 Views
  • 1 replies
  • 1 kudos

FLASH data temperature resistance

Good day!The question is:What temperature and for how long time I can heat BLUENRG-132 after programming without breaking the data ? In the experiment, data is saved after soldering. But, I want to understand where this is written in the documen...

S2-LP + BALF-SPI2-01D3 output power linearity

Hello,we have developed some custom boards with S2-LP transceiver and BALF-SPI2-01D3 balun coupled. We notice a non-linear behaviour between the output power set to s2-LP and the measured output. By direct connection between signal analyzer and S2-LP...

MMerl by Associate
  • 578 Views
  • 0 replies
  • 0 kudos

Help in Balun filter package

Hi We are using BlueNRG-MS IC for BLE communication, in that we are facing issue with Balun filter IC package. BALF-NRG-01D3 /02D3 having  CSPBGA package which we are unable to solder, so we are looking for alternate package or any alternate method f...

Skada.3 by Associate III
  • 539 Views
  • 0 replies
  • 0 kudos

S2-LP trying to get CSMA/CA working

Hi everyone,I am trying to set up CSMA/CA on the S2-LP.Depending on the rssi threshold (RSSI_TH) it may be functional or not.If I set RSSI_TH very low, data packages are not transmited and I get the interrupt "Max.number of back-off during CCA". As e...

BKess by Associate II
  • 1629 Views
  • 2 replies
  • 0 kudos