cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-STLKT01V1 GATT_Init failed

Sam Ho
Associate II

Hello,

I am using the first generation STEVAL-STLKT01V1, I have complied and downloaded the BLE_SampleApp onto the board. I cannot connect to the board using the app.

Below are the debug output from the consol

STMicroelectronics STLBLE1:

    Version 2.0.0

    SensorTile

OK Temperature Sensor2

OK Pressure Sensor

Enabled Temperature Sensor2

Enabled Pressure Sensor                 

    (HAL 1.8.2_0)                  

    Compiled Mar                   

GATT_Init failed                     

                             

Error while adding HW Service W2ST

Error while adding Config Service W2ST

Many thanks,

Sam

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Winfred LU
ST Employee

Hi Sam,

Tested STEVAL-STLKT01V1 with STSW-STLKT01 v2.0.0

and it worked properly for me.

Below would be the output prints:

STMicroelectronics STLBLE1:
        Version 2.0.0
        SensorTile
OK Humidity Sensor
OK Temperature Sensor1
OK Temperature Sensor2
OK Pressure Sensor
Enabled Humidity Sensor
Enabled Temperature Sensor1
Enabled Temperature Sensor2
Enabled Pressure Sensor
        (HAL 1.8.2_0)
        Compiled Apr  8 2019 15:24:19 (IAR)
        Send Every  500mS Temperature/Humidity/Pressure
Debug Connection         Enabled
Debug Notify Trasmission Enabled
SERVER: BLE Stack Initialized
                Board type=SensorTile HWver=49, FWver=7.1.e
                BoardName= STLB200
                BoardMAC = c0:78:3e:34:51:38
 
HW      Service W2ST added successfully
Config  Service W2ST added successfully

Sam Ho
Associate II

Turns out i have a broken board