cancel
Showing results for 
Search instead for 
Did you mean: 

Wireless M-bus Stack source code or older version release availability

tt.353
Associate II

Is there available older version of X-CUBE-SUBG1 package? Where can i download it?

Last version (en.x-cube-subg1_firmware3.1.0 and en.x-cube-subg1_firmware3.0.0) have some problems. I want to read data from WM-Bus meter using T2 mode in "OTHER" mode.

I run example using SPIRIT1 extension board and Nucleo L152RE and it don't work, after i slow down SPI (to 100kHz CLK) i can read data from some wireless meter, i got 3 meters from the same manufacturer and i can read data only from one. Also there is strong dependency of software optimalization on some cases it work on some cases not.

There is version:

binary 2.4.2: libSPIRIT1_wMBus_Library242_CM3_SW4.a

other files 2.4.2 | 2.4.3 | 2.5

In X-CUBE-SUBG1 firmware packet there is many types of library compiled binary files (IAR KEIL on different cortex core)

When i use sample program (precompiled hex for nucleo) from :

STSW-CONNECT009

Wireless M-Bus collector work fine (with 4MHz CLK on SPI). Also when i compile included example in IAR. It work fine here binary library and .h files version is V2.4.3. I can read data from all meter without any problem. There is only one library file WMBUS_Library_2013.lib working with IAR

I need to run this library on SW4STM32 so i can't move binary from working IAR project becourse GCC dosn't recognize .lib library.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0