User Activity

I purchased several X-NUCLEO-IDW01M1 expansion boards. Some boards operate normally, while others reset approximately every 3 seconds and do not operate normally. I don't know if it will help but attach the log.
Sensor-Node (FP-SNS-6LPNODE1) - Wifi Bridge(FP-NET-6LPWIFI1) ​Is there any way to send a message like HTTP Get to the web server via Wifi Bridge?Sensor-Node needs to send an http get message to the web server, which is not good.
FP-NET-6LPWIFI1 The wifi-bridge application is being changed to the S2LP Module. SubGHz_radio_driver.on (); Forever run..Any suggestions?
The B-L475E-IOT01A contains the spsgrf-915 module. I want to use this without an extension board to run FP-NET-6LPWIFI1. Is it possible? It is necessary to refer to it if possible.