Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sensor Tile firmware stop working after a couple of debug connections - SysTick_Handler is never triggered.

After a couple of times that I reflashed the unit to debug, it became unresponsive. The first few times I got to download and debug the Sensor Demo project, the it stopped working alltogether. I got to connect the debugger and go step by step. In the...

WFerr.1 by Associate
  • 508 Views
  • 0 replies
  • 0 kudos

blueNRG-2 deep sleep issue workaround

Hi All,I am using "blueNRG-2" MCU, I want to configure it to enter the deep sleep mode.The issue is when the BLE stack is initialized sometimes I can enter the deep sleep and sometimes I can not.I noticed that whenever I can not enter the deep sleep...

MElna.1 by Associate
  • 731 Views
  • 0 replies
  • 0 kudos

Resolved! FOTA update IoT node kit

I am trying to get FOTA updates working with the IoT node kit and Azure.I currently have v4.0.1 installed on the board. I uploaded v4.0.2 to an azure storage account where I created a blob and uploaded the file, then generated a blob sas url.In my Az...

DSabo by Associate III
  • 1576 Views
  • 2 replies
  • 0 kudos

S2LP StatusByte 0x52 0xE9 error

Hi, I try to transmit data by S2LP(RC-S2LP-433) and have a problem. When I try to debug the unit (true studio) everything work great, when the TX end then get an ISR to reset flag and in main loop start new transmitt. When I try to start the unit wit...

Macias by Associate II
  • 1919 Views
  • 5 replies
  • 0 kudos

How to generate NACK in slave mode?

Hello,I ask connoisseurs of i2s. How to generate NACK in the slave mode if NOSTRECH = 1 and the slave device sends data to the master?If the slave receives data, then there are no such problems. You can wait for the RXDR to overflow and the slave wil...

User.5 by Associate
  • 738 Views
  • 0 replies
  • 0 kudos