cancel
Showing results for 
Search instead for 
Did you mean: 

[SOLVED] Is there a method to update the text in the screen from the main() ?

Ciuffoly
Senior

Also adding these includes it is impossible to modify text in the screen or select a button from the main.cpp - main() - while(1) { }

/* USER CODE BEGIN Includes */

#include <stm32746g_discovery_qspi.h>

#include <gui/screen1_screen/Screen1View.hpp>

#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>

/* USER CODE END Includes */

/* Start scheduler */

   osKernelStart();

   /* We should never get here as control is now taken by the scheduler */

   /* Infinite loop */

   /* USER CODE BEGIN WHILE */

   while (1)

   {

       /* USER CODE END WHILE */

       Screen1View().setIRBuffer("pippo"); <<<<< NEVER GO HERE !!!

       /* USER CODE BEGIN 3 */

   }

   /* USER CODE END 3 */

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Ciuffoly
Senior

Add the code in Screen1View.cpp where thare are the other touch events like Screen1View::buttonUpClicked().

void Screen1View::handleTickEvent()

{

   if (key == 1) // received event from HW like infrared receiver

   {

       touchgfx::Unicode::snprintf(IRBuffer, IR_SIZE, "Test IR");

       IR.setWildcard(IRBuffer);

       IR.resizeToCurrentText();

       IR.invalidate();

       key = 0;

   }

}