Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RS485 - AN3070 - Example

Hello,I'am using Atollic TrueStudion for STM32 v9.3.0 / (STM32F446ZE)where can I find the sample code from AN 3070 "Managing the Driver Enable signal for RS-485 and IO-Linkcommunications with the STM32 ™’s USART".

RSpil.1 by Associate
  • 1068 Views
  • 1 replies
  • 0 kudos

Is there any example code of using BlueNRG2 SoC in mesh and to exchange data using its UART pins from the virtual terminal ?

I am using Keil for the development and has run GPIO & UART examples given in BlueNRG-1_2 DK 3.1.0The objective is to connect each BlueNRG2 SoC with Microcontroller via UART pins and exchange the information strings in between the microcotrollers usi...

Bhim by Associate
  • 2014 Views
  • 4 replies
  • 0 kudos

Resolved! Power Consumption of bluetooth

is there any documentation out there that tells how much power is being consume when the bluetooth operates?and if the power consumption is affected whether the Device is running on RUN mode or STANDBY mode.If there are any tips that can make reduce ...

reokyouma by Associate III
  • 1557 Views
  • 2 replies
  • 1 kudos

How to get access to the blueNRG-2 source code?

Hello,I'm using a STEVAL-BCN002V1. I would like to be able to change the security levels (since BLE mode 1 has 4 security levels) to check if the battery consumption changes or not and also to implement a code to modifiy the security level according ...

GLAUD.1 by Associate
  • 875 Views
  • 1 replies
  • 0 kudos

Cannot debug BLUENRG-TILE using Atollic IDE

using STEVAL-BCN002V1, with ST-LINK/V2 and Atollic IDE. Cannot enter the debug mode. Gives a hardfault error. Using BLE_sensordemo , downloaded from ST website. This should work .Also tried downloading BLE_Sensordemo.hex usint the STSW-BNRG1STLINK ut...

JD'Ad.1 by Associate
  • 621 Views
  • 0 replies
  • 0 kudos