Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Glue which contains phthalates is used in IC. Percentage of phthalates (DBP) is exceeded allowed threshold level stipulated by EU RoHS directive. - Does the DBP evaporate during manufacturing process?

Hi, I got material compliance from Silicon Expert Database. Concerned part is an IC. According to Silicon Expert, there is glue used for die attach. The glue contains a phthalate based substance, DBP. DBP use is restricted by EU RoHS directive, via d...

ADres.2 by Associate
  • 749 Views
  • 0 replies
  • 0 kudos

Resolved! S2-LP packet loss and DMA Rx infinite loop

Hello,I use two X-NUCLEO-S2868A2 board with blueNRG-2 with BlueNRG-1_2 DK 3.2.1 and S2-LP_DK_1.3.2I use following RF configuration :#define MODULATION_SELECT MOD_2GFSK_BT1 #define DATARATE 50000 #define FREQ_DEVIATION ...

0693W000008wyDrQAI.png
AndyR1 by Senior
  • 1144 Views
  • 3 replies
  • 0 kudos

I'm doing a project with a steval-idb008v2 and I have a doubt due to a small note. Can the steval-idb008v2 be reprogrammed with a code created specifically by the user?

the note says this: The STM32L microcontroller on the board is not intended to be programmed by users. ST provides a preprogrammed firmware image for the sole purpose of interfacing BlueNRG-1, BlueNRG-2 to a USB host device.

ASpar.1 by Associate II
  • 863 Views
  • 1 replies
  • 0 kudos

S2-LP / FKI433V2 is receiving garbage data from 433Mhz ASK Manchester Encoded 9.6KBaud transmitter using S2-LP DK GUI.

 I have tried setting the MANCHESTER_EN register and a huge combination of data rates etc in order to get some sensible data in the S2-LP GUI, but nothing is consistent or representative of the data I expect to see.I can see the data correctly using ...

0693W000008yBlyQAE.png
CKild.1 by Associate
  • 877 Views
  • 1 replies
  • 0 kudos