cancel
Showing results for 
Search instead for 
Did you mean: 

BLUENRG2 M2SP interface with SPI protocol As Network processor , i sending Write Command its Responding Wrong Response instead 02 , its responding Wrong Data , Can we Get SPI command and Response pdf of its support to BLE 5.0 specification

mkuma.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Wingunder
Associate III

Hi mkuma.1,

I could also not find any SPI command-response documentation For the BlueNRG2 MSP / MSA.

However, if you install the BlueNRG-1_2 DK 3.2.1 software package. You need Windows or wine (on Linux) to do this.

Browse the BlueNRG-1_2 DK 3.2.1 software and look in the BlueNRG-1_2 DK 3.2.1/Project/BLE_Examples/DTM directory.

The DTM_cmd_db.h and DTM_cmd_db.c files would probably help you further.

Why is the BlueNRG-1_2 DK 3.2.1 package is not just packaged in a simple .zip file?

Regards

***Edited by moderation*** - please note that the admins of this community are not technical experts and, therefore, are unable to help with technical questions. The appropriate team has been notified of your post for assistance.

mkuma.1
Associate II

Hi Wingunder

Thanks for your Response , i resolved spi issue .

Regards

Manukumar