Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Enter deep sleep problem of the BlueNrg-2 FreeRTOS

Please let me know below the below status and can't enter deep sleep by Bluenrg-2 FreeRTOS. ​1.vPortSuppressTicksAndSleep( TickType_t xExpectedIdleTime )2. BlueNRG_Sleep(SleepModes sleepMode, uint8_t gpioWakeBitMask, uint8_t gpioWakeLevelMask)3.ble_s...

CKim.18 by Associate II
  • 1751 Views
  • 2 replies
  • 0 kudos

BlueNRG gdbserver for ST-LINK V3

Hello all,I’m just getting started playing around with BlueNRG 1 & 2 devices. I’d like to be able to debug with an ST-LINK V3 not using uVision. I found a patched ST LINK gdbserver in the 3.2.1 DK download but it’s an old version that doesn’t seem ...

svcguy by Associate III
  • 1188 Views
  • 1 replies
  • 0 kudos

S2-LP getting into unknown state (MC_STATE0 is 0x29)

Greetings, I'm configuring the S2-LP to act as a receiver and then strobing the reception. Sometimes the reception works and the S2-LP goes to the RX state as seen from the first 2 bytes of status on MISO . Sometime, randomly, it goes into an unknown...

PNare by Associate III
  • 4215 Views
  • 7 replies
  • 1 kudos

Hi everyone, does someone know an example of communication of CANOPEN and which evaluation kit iwith STM32 is possible to use it?

For my project, I would like to create a communication (CAN and CANOPEN) with an evaluation kit of ST and an other electronic card and a sniffer to analyse the different weft in the bus. But I'm a novice in this communication so I search an example o...

CMahe.1 by Associate II
  • 672 Views
  • 0 replies
  • 0 kudos

L6362ATR - MTBF/FIT

Hello,can you please provide reliability data (at least a FIT value) for the L6362ATR ?A document would be nice.Best regards,Markus

MNeum.1 by Associate II
  • 809 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-IDP004V1 connection with STM32 Nucleo

Dear Supporters,iam purchanging a STEVAL-BFA001V1B kit and STEVAL-IDP004V1 IO-Link master Board,now i wanted to connect my IO_Link master Board to STM32 Nucleo Board and use Nucleo Board as main Controller. is it possible for data transfer between IO...

GVall.2 by Associate II
  • 2588 Views
  • 4 replies
  • 0 kudos