Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 UART1 most significant part problem

Hi,I'm trying to use uart1 in stm32f411ce and I have a weird problem. in my test I am sending data from the stm32 to an arduino and printing the received data on the serial monitor. In the stm32 I'm sending bytes with the most significant part counti...

0693W00000DqIsqQAF.jpg
EPora.1 by Associate II
  • 3433 Views
  • 13 replies
  • 0 kudos

Maximum NVM write cycles for the STUSB4500

My application makes use of 4 different PDOs but the STUSB4500 can only store 3, to get around this I reprogram the NVM whenever I need access to the fourth. I'm keeping a counter for the number of rewrites so that I can issue a warning when I approa...

JCart.3 by Associate
  • 891 Views
  • 0 replies
  • 0 kudos

STLINK-V3MODS use the VCP

Hi everyone,I see there are differences between V3MODS und V3MINI in the assembly, jumpers etc.Do I need to assemble any jumpers to make the V3MODS VCP run on CN2 Connector?Best regards,Mathias Brandl

mathias by Associate II
  • 965 Views
  • 1 replies
  • 0 kudos

Resolved! BlueNRG2 OTA Flash verify failure

HelloI'm trying to implement the OTA feature in my project. We use the BlueNRG-2 Chip.I'm followed the BLE_Chat example and the explanaition in the The BlueNRG-LP (over-the-air) firmware upgrade document to inlcude all the ota related code parts.When...

TGats.2 by Associate II
  • 2728 Views
  • 5 replies
  • 1 kudos

BlueNRG-X Flasher Utility (4.1.0) is not recognizing SWD connections when ST-link/V2 is connected. I'm running the flasher through a command line interface to get the error message (BlueNRG-X_Flasher_Launcher.exe).

The error message that appears is:"Traceback (most recent call last): File "Script_launcher.py", line 542, in <module> File "globals.py", line 555, in get_stlink_list File "build\bdist.win32\egg\usb\core.py", line 1246, in device_iter File "build...

0693W00000D1efmQAB.png
VLima.1 by Associate II
  • 3319 Views
  • 5 replies
  • 0 kudos