Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Measuring the reliability of mesh network

I want to measure the reliability of bluetooth mesh network. I am using two STEVAL-IDB008V2 boards , one STEVAL-IDB007V1 board and an android smartphone to construct a bluetooth mesh network and using the lighting demo project of STSW-BNRG-Mesh v 1.0...

MH1 by Associate II
  • 4399 Views
  • 7 replies
  • 0 kudos

S2-LP GUI base frequency and Synth value

Dear,having started 2 S2-LP evaluation boards and setting the base frequency in the GUI to 915 MHz. 1ste S2-LP calculates 914.999.999 Hz and second one calculates 915.000.004 Hz with corresponding Synth register values 0x02 0x49 0x98 0xF8 hex and 0x...

PPelg.1 by Associate
  • 775 Views
  • 0 replies
  • 0 kudos

M41T62 RTC Alarm

Hello, We are currently using the M41T62 RTC which is connected to a STWINKT1B board from ST along with the drivers meant to be used with M41T62(download page).We have been successfully able to use it to set a 1 min alarm with interruptions in repeti...

Where can I finfd the SPWF01S firmare packages STSW-WIFI001? I need to upgade the firmware of the X-NUCLEO-IDW01M1 expansion board

Hello, I'm trying to upgrade the firware of the SPWF01S. In the upgrading manual it's says that I need a binary file to program the flash. I saw that the package was avaible in the following link, but now that page doesn't exists. From where can I do...

Javi by Associate
  • 1046 Views
  • 1 replies
  • 2 kudos

Unable to connect to board using Unico GUI

I have 6 of these dev boards. one of them i bought before the other 5. for the later one the STEVAL -MKI205V1 dev board I'm trying to test is returning a "ERROR: The adapter board has not been recognized, the WHO_AM_I register value does not match th...

0693W00000D1f0kQAB.png
YFels.1 by Associate
  • 865 Views
  • 0 replies
  • 0 kudos