User Activity

Hello We're using BlueNRG-2 VTimer to be RTC for wake-up the system when it's in sleeping mode.when we set the timer 10mins, it still wake-up the the system every 15 sec.HAL_VTimerStart_ms(0, 600000);But I don't turn on the other timer such as 1 or 2...
Hi,I'm using EVK (STEVAL-FKI868V2), loading the Binaries file to EVK All the command line function is ok. but when I use your sample code:File Location: C:\Program Files (x86)\STMicroelectronics\S2-LP_SigFox_DK_1.6.0\Projects\Projects_Cube\S2-LP_SigF...