Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Appears and disappears

hello I have purchased the steval-idp004v2 board and when I connect it with GUI V2 ST and with the TE concept IOlink application, the same error appears master application 6148 Appears i Disappears. Thank you for response

MLuna.1 by Associate
  • 1382 Views
  • 2 replies
  • 3 kudos

Which example code should I use?

Hi Friend,We have an old project using BlueNRG-1. The project is peripheral. Now, we want to modify it to a new project. The new project has a custom 128-bit uuid and two 16-bit uuids. Two 16-bit uuids are based on the above-mentioned 128-bit uuid. O...

TWu.6 by Associate II
  • 1364 Views
  • 2 replies
  • 0 kudos

BlueNRG beacon frame interleaving

Hi,I'm trying to implement an Eddystone beacon with interleaving frames, e.g. UID + TLM, using a BlueNRG-MS and BlueNRG-2. I can configure the BlueNRG to act as a beacon broadcasting one of these frames but I don't see how to go about alternating or ...

jaylong by Associate II
  • 2467 Views
  • 6 replies
  • 0 kudos

Enabling OOB pairing on the blueNRG1

I'm trying to use OOB pairing with the blueNRG1, using the latest DK3.2.1 (stack V2.1c). There is no example available, the security example has all security examples with exception of OOB. I'm trying to use LE legacy mode for now, but LE secure is ...

allard by Senior
  • 1535 Views
  • 2 replies
  • 1 kudos

STM32 UART1 most significant part problem

Hi,I'm trying to use uart1 in stm32f411ce and I have a weird problem. in my test I am sending data from the stm32 to an arduino and printing the received data on the serial monitor. In the stm32 I'm sending bytes with the most significant part counti...

0693W00000DqIsqQAF.jpg
EPora.1 by Associate II
  • 3348 Views
  • 13 replies
  • 0 kudos